El Grupo Endress+Hauser

Sala de prensa

Eventos

Su carrera profesional en Endress+Hauser

Herramientas

Información de contacto

E-direct Shop

E-direct complementa la gama tradicional de Endress+Hauser, ofreciéndole instrumentación económica, fácil de instalar y configurar.

E-direct Shop

Industrial Ethernet Training PROFINET

A hands-on based course, recognized in all industries

By becoming familiar with the PROFINET protocol you will learn about the advantages of PROFINET technology as well as procedures for troubleshooting.
At the end of the course you will be able to plan a PROFINET system and bring it into operation. The course focuses on the link between PROFINET and PROFIBUS PA as well as HART.

Índice de contenidos

  • In the theoretical part the following content is covered:
    ISO/OSI model, types of wires and components, network structures and network calculations and
    grounding and shielding concepts.

  • Drivers, name assignment and addressing, commissioning procedures and troubleshooting procedures.

  • In the practical part the following content is covered:
    Wiring of PROFINET networks, device setup, commissioning of an own PROFNET network, troubleshooting a PROFINET network.

Objetivos

  • At the end of the course you will understand PROFINET networks in an industrial environment. You will learn about the benefits of PROFINET technology in industrial applications, but also about possible outside influences.

¿Quién debería asistir?

  • Technicians/Maintenance Technicians

  • Service/Support Specialists

  • Supervisors

  • Programmers/Device Configurators

  • Engineers

Requisitos previos

Basic knowledge of electronics and ability to use a computer.

Cualificación

The training is Endress+Hauser certified.

Metodología de evaluación

Participants are given time to work with the various components of a PROFINET network.

We put emphasis on a balanced approach to theory and practice as well as a vendor-neutral atmosphere.

Mornings are spent learning the theoretical background and afternoons with the actual components and integration of the field devices into the system.
Almost half the course is spent on giving you ample opportunity to use what you have learned in hands-on tasks taken straight from our experience.

Tipo

A hands-on based course, recognized in all industries.

Contacto

Endress+Hauser Process Solutions AG
Christoph Merian-Ring 12 CH-4153 Reinach Suiza
Tel.: +41 (0) 61 715 73 78
Enviar correo electrónico www.endress.com