Title

Intente buscar por palabras clave, código de producto/pedido o número de serie, por ejemplo, "CM442" o "información técnica"
Introduzca por lo menos 2 caracteres para iniciar la búsqueda.
  • Historial

Scaling Direct Air Capture for a net-zero future

DACMA's innovative carbon capture systems are designed to efficiently remove CO2 from ambient air. Reliable measurement from Endress+Hauser helps ensure process performance at scale.

Industria: Múltiples industrias
Containerized Direct Air Capture solution from DACMA

Resumen

As industries work toward a climate-neutral future, technologies that actively remove carbon dioxide from the atmosphere are gaining importance. Direct Air Capture (DAC) offers a way to capture CO₂ directly from ambient air, creating new opportunities for carbon removal, utilization and storage. At the forefront of this innovation is DACMA, whose scalable DAC technology is designed to maximize CO₂ uptake while minimizing energy demand, helping transform ambitious climate goals into practical industrial solutions.

The results:

Verification

Every metric ton of CO₂ measured is quantifiable

Uptime

Every sensor failure is detected before it causes downtime

Process optimization

Every measurement feeds into real-time control of the plant

Digital twin

Every plant module is digitally mapped for predictive maintenance

Without precise measurement data, there can be no verifiable impact on the climate: Accurate tracking of energy consumption and CO₂ capture is key to the success of Direct Air Capture (DAC) systems - from regulatory approval to industrial-scale deployment. The measurement data from the plant provides DACMA with a clear basis for decision-making regarding the technology’s further development.

Adrian Kortmann, Project Manager at DACMA, in front of their containerized DAC unit

"As our systems evolve and scale, Endress+Hauser continues to support us with reliable instrumentation, technical know-how and a partnership approach that helps us tackle new challenges together."

Adrian Kortmann, Project Manager, DACMA GmbH
Frederik Effenberger in front of flow meter installed in containerized Direct Air Capture unit

"We are proud to support DACMA on their journey: With precise measurement technology, global expertise and a true partnership. For a climate-neutral future."

Frederik Effenberger, Industry Manager Decarbonization, Endress+Hauser

The challenge:

For Direct Air Capture (DAC) systems, process performance is defined not only by the amount of CO₂ captured, but also by the ability to quantify carbon removal with a high degree of accuracy. Reliable measurement data is essential for verifying capture rates, assessing process efficiency and establishing the transparency required by investors, regulators and carbon markets.

DACMA faced the challenge of measuring high-purity gaseous CO₂ under varying operating conditions while maintaining a compact system design. The instrumentation needed to deliver stable and accurate measurements without imposing complex installation requirements, ensuring seamless integration into the capture process.

Beyond CO₂ flow measurement, a comprehensive understanding of plant performance requires the correlation of multiple process variables, including pressure, temperature and energy consumption. Together, these parameters provide the operational insight needed to optimize capture efficiency, validate system performance and support the scale-up of DAC technology from pilot installations to industrial deployment.

Our solution:

Delivering process transparency and real-time data

To support accurate CO₂ quantification and energy monitoring, DACMA worked closely with Endress+Hauser to develop a tailored measurement concept. Together, the teams defined critical process parameters, identified key measurement points and selected technologies capable of providing reliable data under demanding operating conditions.

Promass Coriolis flowmeters enable high-accuracy measurement of gaseous CO₂, while additional instrumentation, including Prowirl vortex flowmeters for steam, Promag electromagnetic flowmeters for condensate flow and Liquicap for level measurement, provides visibility into key utility and process streams.

By combining these measurements, DACMA can correlate mass and energy balances across the entire process. This integrated data foundation supports process optimization, validates system performance and provides the transparency required to scale Direct Air Capture technology from pilot projects to industrial deployment.

Products and services used

/

Related solutions and technology

Medición de la temperatura

Sondas de temperatura y transmisores para la industria de procesos

Más información

Productos de sistema

Gestores de datos y componentes adicionales. Visión general del producto - Soluciones para el lazo

Más información

Soluciones de software

Aparte de todas las tecnologías de sistema y medición relevantes, también ofrecemos aplicaciones de software apropiadas para todos los sectores industriales a los que proveemos para que ejecuten sus procesos operativos a su máximo potencial.

Más información

Medición de presión

Medición de presión y presión diferencial para líquidos, gases y vapores

Más información

Monitoring of effluent discharge 

Operate wastewater discharge within legal limits with complete, reliable monitoring for continuous values and fast response to contamination.

Read more

Hydrogen measurement in natural gas pipelines

Fast, continuous hydrogen measurement in natural gas pipelines enables safe blending, quality compliance and dynamic control using Raman spectroscopy - without consumables or flaring

Read more

Biomethane quality analysis for safe and compliant gas injection 

Ensure reliable biomethane quality with fast, accurate online measurement of H₂S, water dew point and critical parameters for safe grid injection and efficient operations. 

Read more

Protect reverse osmosis membranes with online water quality monitoring for desalination 

Reliable online water quality monitoring to protect RO (Reverse Osmosis) membranes, reduce cleaning effort, and extend membrane lifetime in desalination and water reuse applications

Read more

FAQs

Logo de la compañía: DACMA GmbH

DACMA GmbH, con sede en Hamburgo, desarrolla y opera sistemas de Captura Directa del Aire (DAC) para la eliminación de CO₂ atmosférico. Gracias a la combinación de conocimientos en ingeniería mecánica, de procesos y aeroespacial, la empresa ofrece tecnologías de emisiones negativas robustas y escalables. Con un equipo interdisciplinar y proyectos internacionales —incluidos algunos en Brasil— DACMA impulsa el despliegue industrial de la DAC y contribuye al avance de los objetivos climáticos globales.