Intente buscar por palabras clave, código de producto/pedido o número de serie, por ejemplo, "CM442" o "información técnica"
Introduzca por lo menos 2 caracteres para iniciar la búsqueda.
  • Historial

A win for everyone

Sustainability should be worthwhile commercially. That’s why Endress+Hauser’s approach to decarbonizing its portfolio combines climate protection with added value, delivering even greater benefits to the customer.

01.06.2026 Texto : Christine Böhringer Fotografía: Andreas Mader
Space-saving design gives Compact Line instruments a comparatively small carbon footprint.

Endress+Hauser has set a goal of net-zero greenhouse gas emissions by 2050. The biggest challenge in achieving this lies in the Group’s up- and downstream value chains, with Scope 3 accounting for the bulk of its greenhouse gas emissions. Hans Joachim Fröhlich, Technology & Portfolio Director, explains: “We use a lot of steel and aluminum in our instruments, so more than a third of our environmental footprint comes from bought-in goods. And about half the footprint is attributable to energy consumption and other factors during the customer use-phase of our instruments, when you consider their long service lives.”

Hans Joachim Fröhlich, Technology & Portfolio 
Director. ©Endress+Hauser

For these reasons, Fröhlich is working with Endress+Hauser’s product centers to decarbonize the Group’s portfolio. “We’re reviewing our portfolio product by product. We want the next generations of our instruments to be more sustainable while also giving customers added value – in the form of improved performance at a fair price, or unchanged performance at the same or lower prices.”

To shape this innovation process, the company is rolling out new group-wide ecodesign guidelines. The framework forms part of company standards for product development and will in future direct over 1,300 R&D personnel in their work. It lays down ecological principles and practices while still allowing latitude for designer creativity. The aim is to optimize the design of various types of instruments, focusing on aspects including the metals used, materials savings, the electronics, energy consumption and, in the case of analyzers, the emission levels of test gases. Endress+Hauser also intends to further boost its measuring instruments’ repairability and recyclability in the drive toward a circular economy.

Shorter development timeframes

In the future, software tools will help the company’s development teams assess the environmental implications of their ideas. Such tools could, for example, be used to identify the energy mix that goes into producing the proposed materials from which an instrument will be manufactured. There will also be greater use of technologies for testing and optimizing design variants virtually – before the first prototype is even built. “We are already industry leaders when it comes to simulating the behavior of components made from new eco-friendly and low-emission materials,” explains Hans Joachim Fröhlich. The development teams can also use computer simulation to rapidly assess the performance and commercial viability of new components, assemblies and entire instruments.

In Fröhlich’s view, achieving the company’s net-zero emissions target and, more specifically, realizing the optimal pairing of ecological sustainability and commercial viability will require both digitalization and close partnership with suppliers. Like Endress+Hauser, those suppliers are continually optimizing their processes, and many already operate very progressive value chains relative to their industry peers. “All of this is helping us to accelerate sustainable innovation for the benefit of our customers and the attainment of our bold climate goals,” says Fröhlich. Endress+Hauser aims to achieve a 35 percent reduction in emissions from its up- and downstream value chains by as early as 2034.

Sustainability by design

With its new ecodesign guidelines, Endress+Hauser is embedding sustainability principles even more deeply into its innovation processes. The framework ensures early-stage consideration of ecological factors in new product development and redesign of existing ones. The aim is to minimize the environmental impacts of the company’s products – by focusing on the type of construction or the materials and components used, for example. Good ecological design always creates environmental as well as economic benefits, such as through material savings or lower operating costs. The new framework aligns with the recent EU Ecodesign Directive and harmonizes existing standards within the Endress+Hauser Group.

In good shape

Endress+Hauser already offers reduced-emission measurement technologies,
with new housing and electronics designssaving energy and materials. Here are three examples.

Dosimag and Dosimass

Dosimag and Dosimass flowmeters have been in use for three decades across a wide range of filling and dosing applications – from ketchup and champagne to cough syrup. The latest generation reduces the carbon footprint by up to 14% and 28% (for Dosimass and Dosimag respectively), supported by material savings and locally sourced components. The instruments also consume less energy. In addition, the Dosimass transmitter is now easier to recycle, as the electronics can be separated from the sensor.

Proline transmitters

One variant of Endress+Hauser’s product family of Proline transmitters for flowmeter systems ships in quantities of 50,000 units a year, all with the same aluminum housing. In late 2024, the wall thickness was reduced, saving around 14 tonnes of aluminum annually, equivalent to about 150 tonnes of CO2. The new housing was developed using numerical simulation and high-pressure die casting, ensuring it meets the same mechanical specifications as the previous version.

Compact Line

Endress+Hauser is a long-time producer of level and pressure measurement instruments for hygiene‑critical applications. The new Compact Line is specifically designed for requirements in the food & beverage and life sciences industries, offering high‑performance, space‑saving housings and electronics. This results in a markedly reduced carbon footprint compared with conventional products. In the case of radar measurement instruments, the saving is about 60 percent.

Leer sobre temas similares

Descargas

Explorar otros recursos

document icon
Revista corporativa 'changes' 1/2026 PDF, 7.5 MB
Moldeando la transformación sostenible
download icon Descarga